Hi
I am running LPCOpen ADC example and after downloading code to MCU I read this message in the MCUXpresso command line:
"[MCUXpresso Semihosting Telnet console for nxp_lpcxpresso_11c24_periph_adc.axf started on port 3330]"
Q: What command should I use in Telnet console to connect to the board.
Thanks
Regards, Adam
Solved! Go to Solution.
That's the semihosting output console - not one for UART/VCOM output. If you want to display output sent via the UART/VCOM, you'll need to use a separate terminal program.
Alternatively, if you want to modify the application to send output via semihosting, then details of how to modify your LPCOpen package can be found in the MCUXpresso IDE v10.0.0 User Guide, section 11.5.4, "Printf when using LPCOpen".
Regards,
MCUXpresso IDE Support.
That's the semihosting output console - not one for UART/VCOM output. If you want to display output sent via the UART/VCOM, you'll need to use a separate terminal program.
Alternatively, if you want to modify the application to send output via semihosting, then details of how to modify your LPCOpen package can be found in the MCUXpresso IDE v10.0.0 User Guide, section 11.5.4, "Printf when using LPCOpen".
Regards,
MCUXpresso IDE Support.
Thank you for the prompt reply !
The section 11.5.4, "Printf when using LPCOpen" helped.
Is it possible to redirect/access the output from the IDE console by external application ? I would like to plot the values in eg Qt. I think it would require some MCUXpresso API and dll that can be linked to other PC based application.
This might be a candidate for a new question.
Thank you.
So the simple way would be to copy out the contents of the semihosting console and paste into an external text editor. See section 14.7.2, "Copying the contents of a console" of the MCUXpresso IDE v10.0.0 User Guide.
Regards,
MCUXpresso IDE Support
"So the simple way would be to copy out the contents of the semihosting console and paste into an external text editor. "
I did that but I would like to see a plot in 'real time'.
Is the answer to my question
"Is it possible to redirect/access the output from the IDE console by external application ?"
no ?
Hi Adam,
Does your external application can receive data though a serial port? Maybe it would be easier to redirect the output to be sent via the UART/VCOM and use this communication channel instead.
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer
Hi Carlos,
Thank you for the reply.
There is not yet external application. I have experience with Qt/CAN combo so that might be a solution. And my application will need CAN anyway.
I tried to use semihosting but a simple line in ADC example eg
DEBUGOUT("%d", sample);
takes cca 75ms to execute on MCU(to send data to the MCUXpresso command line). And interrupts are disabled during this operation .
This makes me think if everybody writes his/her own tool on PC to get/set data from/in the MCU application, to plot data to see trends etc. I worked for big company before and had a special tool that did that. Now I work alone and starting from the bare metal and think how to debug/test my application.
Regards, Adam
Carlos,
I want to add to what I wrote that it is about debugging embedded SW in general, not in relation to NXP tools/MCUs.
Cheers, Adam
Hi Adam,
One of the disadvantages of semihosting is that it is rather slow (only several hundreds of bytes per second) because it needs debugger interactions. If you still want to use semihosting there is a faster approach using Segger Real Time Terminal (RTT), you can find more information on this post:
Using Segger Real Time Terminal (RTT) with Eclipse | MCU on Eclipse
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer