AnsweredAssumed Answered

Do the RGMII reference clock inputs,  EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040 have to running at boot time or can they be enabled after boot?

Question asked by Al Duarte on Jun 16, 2017
Latest reply on Jun 19, 2017 by Serguei Podiatchev

Do the RGMII reference clock inputs,  EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040have to running at boot time or can they be enabled after boot? .  I need to know if those two clocks have to be running at power up or if they can be enabled after boot up.

Outcomes