Can i program qn9021 using swd of general arm Jtag?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i program qn9021 using swd of general arm Jtag?

653 Views
pranaykotha
Contributor I

I made a breakout board for qn9021 using dc-dc converter circuit from the data sheet. From software developers guide, I found that all qn9021 comes with preloaded small bootloader which can be used to flash program over spi or uart. I tried using usb to ttl by setting all the possible baudrates, everytime i got error "connection timed out". What might be the problem. Will it be succesfull if using general arm jtag to program it?

0 Kudos
1 Reply

534 Views
antonioconcio
NXP Employee
NXP Employee

Hello,

Please be sure you are using the correct pins : QN902x’s PIN0_0 and PIN1_7 are used as UART ISP interface; PIN1_0, PIN1_1, PIN1_2 and PIN1_3 are used as SPI ISP interface.

And yes, standard SWD interface/programmer can be used.

Cheers,

Antonio

0 Kudos