Hello,
I am using T1042 processor for my board. I have to use two SATA interfaces, all four PCI express interfaces and two 1G Ethernet Interface. My question is that is there any possibility that I can use them without using SERDES ? If I had to use SERDES, then which channel for which interface and how ?
Thanks in advance.
Regards,
Ather
So I can not use four PCIe, two SATA and two Ethernet at a time ?
Possible combination is Three PCIe, two SATA and three Ethernet interface.
Thanks Ufedor,
What I have to do if I want some configuration that is not listed in the Figure 31-1 ?
for example I want 4 PCIe, two SATA and two ethernet interfaces
All supported configurations are shown in the Table.
The SerDes is used for each high-speed serial interface.
> which channel for which interface and how ?
Please refer to the QorIQ T1040 Reference Manual, Chapter 31 SerDes Module, Figure 31-1. Supported SerDes Options.