Is there a way to use UDP under SMAC on the KW24D platform? It seems like that there is that ability on the KW41Z pltform, BUT looking through the MKW2xD_ConnSw_1.0.1, it doesn't look like it. I have received vague impressions from Freescale/NXP that I should be able to do this, but I can't quite get this pinned down.
Hello George,
SMAC doesn't support UDP. However, the Thread protocol does. Please refer to chapter 8 Socket Commands
of the Kinetis Thread Stack Shell Interface User Guide document located in <Conn SW path>\docs\wireless\Thread\ for information on how to open a UDP socket from the shell interface.
Also note that the latest version from the Connectivity Software is v1.0.2
Regards,
Gerardo