I have started working with MPC5604EKIT. As per the quick start guide, I connected Ethernet cable and tested streaming using the url 'udp://@:1234' as mentioned in the quick start guide. I was able to see udp stream in vlc media player. It was in JFIF format and it doesn't have time-stamp.
I am going to work on an application which will have multiple MPC5604EKIT and I will be using its multiple camera synchronization feature as well. Please help me to set up the Ethernet streaming application in MPC5604EKIT which has the Precision Time Protocol support.