Hello all,
I am going to use DSPI links. I am trying to use MPC5777M DSPI sample available in NXP community on a MPC57XX_MB and MPC5777M_512DS.
I have put a breakpoint on the while testing the SR and I have seen that DSPI_0 SR.TCF is 1 and DSPI_2 SR.TCF stay to 0.
The POPR register are set to 0 for both DSPI.
Have you an idea ?
By the way, no modification has been done in the code.
Thanks a lot
Hello
After code deep analysis, I have found that the comment in the main.c header is wrong.
the line : * EVB connection: P18.12 to P14.13 (CS_0)
must be replaced by * EVB connection: P8.12 to P14.13 (CS_0)
By connecting the CS_0 to PA[12] the sample is working well.
Alain
Hi,
Thanks for notification.
We will check it.
Peter