dear NXP team,
I am testing the temperature sensor function in MPC5674F using the EVB board.
I searched the community and downloaded the example code(Example_MP5674F-TSENS-Temperature_cal),
I loaded the sample code on the target board and run it.
The measured TSEN_CODE value were changed between 26 and 32 degree.
I think the deviation is very large, it is normal range?
i wanna know a normal error range.
and, if the measured value is normal, it is difficult to use in my project .
Is there a way to improve accuracy?
Hi, these internal sensors are typically quite imprecise, thus +/-10 °C is valid even it is calibrated in accordance to reference manual.
If you want to measure ambient temperature you should rather use external sensor.