The USB_OTG_VBUS on i.MX 6UL has to be supplied?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The USB_OTG_VBUS on i.MX 6UL has to be supplied?

761 Views
jacopoagostini
Contributor I

Hi, I'm using the processor i.MX 6ULL. I have to communicate through the CPU USB line  USB_OTG_DN e DP; so to do this I need to connect the 5V power supply to the VBUS line. Is it correct?

Labels (1)
0 Kudos
3 Replies

561 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jacopo Agostini,

Yes, if you wish to use the USB module data lines you would need to supply the VBUS line. You may work as Host or Device (in which you may actually receive the 5V voltage from the USB host connected to the i.MX6UL).

I hope this helps!

Regards,

0 Kudos

561 Views
jacopoagostini
Contributor I

Hi, thanks for the answer.

I read on the datasheet that the switchable  resistors used to identify if the processor works as Host or Device, are embedded in the chip (1.5 kohm pull-up and 15 kohm pull-down). These switchable resistors are programmed via software or they automatically change status depending on the system type conncted, that is host or device?

0 Kudos

561 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jacopo Agostini,

You may force the USB OTG module to work in Host/Device trough these programmable resistors as you see fit. In most applications, however, a pin on the USB OTG connector allows the processor to detect whether the peripheral is meant to work as Device or Host.

I hope this helps!

Regards,

0 Kudos