AnsweredAssumed Answered

PTN3363 TMDS input voltage level

Question asked by Matteo Conti on Jun 9, 2017

Hi,

I'm developing an application in which an HDMI signal needs to be shifted up from 1.8V to 3.3V. At page 18 of this document characteristics of PTN3363 are shown: could someone please confirm me that V_RX and V_RX_Diff level range will accept my HDMI input? I'm a bit afraid of what's said on the datasheet "PTN3363 operates only when the input signal level is above certain minimum threshold (as per VRX_DIFFp-p). If the input falls below that minimum threshold, the outputs are squelched."

 

Thank you very much,

Regards,

Matteo

Outcomes