FRDM-K66/26 DWG/Gerber Files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-K66/26 DWG/Gerber Files

440 Views
whata
Contributor III

Hi, 

I've made a custom shield for both of my K66 and K26Z boards and now am in process of making a proper enclosure for both of these boards, however the mechanical documentation is practically non-existent which makes it pretty hard to make a proper enclosure. I believe that the same question has been asked several times, here, for instance. But no proper response was given because the files that were referred to are:

1. Missing the actual *.brd file for the PCB

2. Are in allegro format.  (Which can be viewed by a free viewer but cannot be exported)

Can someone from the kinetis team provide a proper neutral-format file for the K66 and K26 boards, something like a step or dwg file. 

0 Kudos
2 Replies

285 Views
fangli
NXP Employee
NXP Employee

Hi,

We provide the Kinetis Symbols, Footprints and Models from here:

Kinetis Symbols, Footprints and Models|NXP 

We do not provide the whole board gerber file as you asked for. Sorry.

0 Kudos

285 Views
whata
Contributor III

Hi, 

I'm not asking about the gerber sets since I'm not insterested in the layout of the pcb, just the outline of the board. 

0 Kudos