Hi Yuri Muhin ,
I am facing same problem but my kernel version is 3.14.28. In "echo mem > /sys/power/state" after interrupt system is rebooting instead of resume If i use 3.0.35 kernel with that patches it works fine. But my requirement is i should use 3.14.28 kernel. How to solve this issue can you help me
Regards,
Lavanya
Hello,
NXP recommends do not use just SOC reset (OS restart), but - to implement total system POR instead,
via external circuit. For more details please create request (ticket).
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri Muhin,
i.MX6DL LPDDR2 suspend / resume issue with Linux kernel 4.1.15 my problem is similar to this link.
Is there any solution for this like in 3.0.35 it is working https://community.nxp.com/docs/DOC-94922 . similarly can we get any patches or how we can check whether LPDDR2 is in self refresh mode or not.
Thanks in advance.
Regards,
Lavanya