Dear Expert:
I use the i.mx6-sabresd board to test pcie(host).
the linux version:L3.14.52,I have include the PCIe driver through bitake linux-imx menuconfig.
But I can not measure any clock in CLK1_N and CLK1_P.
in command window, input lspci -t ,it will show
-[0000:00]-
So could you tell me how i can configurate when i use the i.mx6 pcie(host)?
thanks for your support.
Hi Tom
one can try to test pcie in uboot, please check #define CONFIG_CMD_PCI in
uboot/include/configs/mx6sabresd.h
uboot-imx.git - Freescale i.MX u-boot Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------