Hi there,
The datasheet of LS1020A says, that pins IFC_A16 - IFC_A20 can be pulled up or tristate (mark 5). Just a requirement - no pull-down.
The application note AN4878 says:
For LS1020A device configuration, IFC_A16 and IFC_A17 must be pulled up
during power-on reset.
Where is the truth? Can these pins be floating or not?
Solved! Go to Solution.
Have a great day,
These pins must be pulled up. As example see the IOT reference board schematics. The IFC_A16 is connected to 4.7k pull-up and to the chip select input of an external QSPI device. They refer to the mark 5 (Data sheet note 5).
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Have a great day,
These pins must be pulled up. As example see the IOT reference board schematics. The IFC_A16 is connected to 4.7k pull-up and to the chip select input of an external QSPI device. They refer to the mark 5 (Data sheet note 5).
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------