AnsweredAssumed Answered

IMX6DL, ONOFF Button press causes RESTART instead of POWER OFF if booting from eMMC

Question asked by Daniel Colon on Jun 6, 2017
Latest reply on Jun 29, 2017 by Rita Wang

The IMX6dl reference manual states that a 5 second press of the ONOFF button should power down the device.  If we boot from an SD card, then everything works correctly and the device powers down.  If we boot from eMMC, then the system going down correctly, but then immediately starts back up.  

 

Anyone have an idea why the boot location would affect the performance?  Are the settings for the eMMC that need to be set in order to enable power down instead of reset?  

Outcomes