Hi,
In the data sheet of both SA602A and SA612A it was specified that the typical local oscillator frequency can be 200 MHz. Can I use them for 250 MHz local oscillator frequency?
If not, is there any other IC that can be used for 250 MHz local oscillator frequency?
Arifur.
Internal LO operation above 200MHz is possible but it is not guaranteed.
You can use external LO signal at 250MHz without problems.
Have a great day,
Pavel
NXP TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------