AnsweredAssumed Answered

IMX6 Sabre Auto SDCard Problem

Question asked by Abdullah Aktay on Jun 3, 2017
Latest reply on Jun 4, 2017 by igorpadykov

Hi all,

I have an imx6 saber ai board.It is booting via SATA but it is not booting from SD card.

I follow the following tutorials.

u-boot on the i.MX6 sabre sd platform in a few commands 

Booting Linux from SATA on i.MX6Q SABRE AI. 

Switch conf for SATA

S2 pin1=>0,pin2=>1,pin3=>0,pin4=>0

Switch conf for SD

S1 pin4=>0,pin5=>1

S2 pin2=>0,pin3=>1,pin4=>0

S3 pin1=>0,pin2=>0,pin3=>1,pin4=>0

 

What could be the problem? Is there any idea?

 

Thanks.

Outcomes