Whether there is an I2C interface in MPC5777C?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Whether there is an I2C interface in MPC5777C?

Jump to solution
962 Views
chenyandong
Contributor II

I need an i2c interface to connect the temperature sensor.

NXP has a spi interface temperature sensor or not.

Another question,whether the eSCI interface can be configured as uart mode for RS232 or RS422.

Thank you.

0 Kudos
1 Solution
793 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I2C module is not present with MPC5777C.

 

For connection of external sensor you may use DSPI module (recommended).

If I2C is necessary then you could possibly also use I2C function running on eTPU module (I would not recommend because number of required pins is doubled). Such function is provided by third-party provider:

https://www.ashware.com/i2c-driver

 

RS232/RS422/RS485 standard is given by version of physical layer connected to device externally, so yes, they can be used with MPC5777C’s eSCI interface.

View solution in original post

1 Reply
794 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I2C module is not present with MPC5777C.

 

For connection of external sensor you may use DSPI module (recommended).

If I2C is necessary then you could possibly also use I2C function running on eTPU module (I would not recommend because number of required pins is doubled). Such function is provided by third-party provider:

https://www.ashware.com/i2c-driver

 

RS232/RS422/RS485 standard is given by version of physical layer connected to device externally, so yes, they can be used with MPC5777C’s eSCI interface.