Hello,
I'm using iMX6DL with Android 5.1.1, Linux kernel 3.14.52. I use LVDS output for display signals. These signals are converted to RGB by an external IC because I use RGB display (only LVDS signals are available from iMX6 hardware).
I'm looking to invert clock polarity of the RGB display. So I tried to invert LVDS clock polarity, which fail until now.
The display is printing the half of screen and blinking pixels. I can see if I stop/enable the good clock source. By default, PLL5 is the clock source.
Ref manual Rev. 2, 04/2015.
- With regaccess, I tried to change some registers, including IPU_DI0_GENERAL, bit 17, di0_polarity_disp_clk => do nothing.
- p810, IPU1_DI0_CLK_ROOT source could be PLLs, ipp_di0_clk, ldb_di0_ipu => when I switch to ldb_di0_ipu (register CHSCCDR:ipu1_di0_clk_sel), screen freezes. What is the source of ldb_di0_ipu ? Which register should I change to invert this clock source ?
Any advice will help.
Thanks, Pierre
Solved! Go to Solution.
Hi Pierre
ldb block produces waveforms like on p.16 hannstar lcd datasheet
http://boundarydevices.com/wp-content/uploads/2014/12/HSD070PWW1-B01.pdf
sect.6.3 Bit Mapping & Interface Definition and clock polarity can not be changed,
regardless of ipu register settings. Seems one can try to interchange LVDS0_CLK_N and P
of external IC.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pierre
ldb block produces waveforms like on p.16 hannstar lcd datasheet
http://boundarydevices.com/wp-content/uploads/2014/12/HSD070PWW1-B01.pdf
sect.6.3 Bit Mapping & Interface Definition and clock polarity can not be changed,
regardless of ipu register settings. Seems one can try to interchange LVDS0_CLK_N and P
of external IC.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------