i.MX 6DQ USB Chirp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6DQ USB Chirp

743 Views
sugiyamatoshihi
Contributor V

Hi, 

I have a question about chirp timing of USB Host connection. 

I think chirp timing like a below.  

I think output timing of HUB K-J Chirp pairs after detecting Device K Chirp controlled by HW  because it must be less than 100uS. 

Is this correct that HW control timing after Device K Chirp?

Best Regards,

Sugiyama

Labels (1)
0 Kudos
2 Replies

580 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

You could refer to “i.MX6/7 Series USB Certification Guide” document regarding this kind of USB specifications of i.MX6 and i.MX7 processors. This document is available at the following link:

http://www.nxp.com/assets/documents/data/en/user-guides/IMXUSBCGUG.pdf


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

580 Views
sugiyamatoshihi
Contributor V

Hi, Carlos,

Thank you for information.

The issue was Hub K-J chirp doesn't start immediately after device K chirp.  However, it was resolved after device move to another board. It sees it was board issue.

Thanks,

Sugiyama

0 Kudos