I need to communicate with my FRDM-25Z board, using the FSL_DEBUG_CONSOLE functions and RTOS. But, I can't find the port configuration to initiate the service.The dbg_init() function doesn't work. Seems to me that I need create the pins configuration to this work. I used the 0u pin to receive data (RX) and 1u to transmit (TX) . the software has no errors, but nothing appears at the serial port, when i use the dbg_putchar() command. I'm using a serial monitor at PC to spy the data, and the baud rate is defined at 115200. Someone has the configuration code to use this?
Hello Marcos,
- Please first be sure the UART port is right .
- The component of "CosnsoleIO" can used to send data through UART:
- If still can't use , please tell me which IDE and which version do you used ?
And also send your project to me , or I don't know where is the "FSL_DEBUG_CONSOLE functions"
and "dbg_putchar() ".
BR
Alice