AnsweredAssumed Answered

Increasing memory size to store variables in FRDM-KL26Z

Question asked by Danyon Chu on May 31, 2017
Latest reply on Jun 16, 2017 by Danyon Chu

I am trying to store a large byte array (size 20-30,000) inside of memory that I receive from another FRDM-KL26z uController over I2C. When I try to store data into that array, I get the 'm_data overflowed by xxxx bytes' error. From what I think is happening is that variables get written to RAM during runtime and I don't have enough of that. What is m_data and is there a way to increase m_data size? Or instead is there a way to write to flash? If that first option isn't possible/feasible, are there any precompiled functions that already do this in the SDK? I am using SDK v1.x and programming using Kinetis Design studio

Outcomes