AnsweredAssumed Answered

the reset value is not correct in SPC5744

Question asked by Xiao LEI on May 26, 2017
Latest reply on May 27, 2017 by Xiao LEI

we now use S32DS to program SPI interface of SPC5744. After reset of CPU, the HALT bit of Register SPI0.MCR is "0" and cannot set to "1" by software. The picture shows the value error of the register. It's really confusing. 

Attachments

Outcomes