Hi,I am working on the customizing board referring to S32V234 evb board.
We use the 2 csi lanes with ov10640 sensor.
It seems to be same configuration with S32V234 evb board.
we use customizing S32 design studio s/w code based on linux.
At the S32 design studio s/w code, the csi driver seems to support 1,2,4 lanes.
so ,I change the csi config value(Lanes = 2 ->4)and ov10640 sensor config value(2->4)
I didn't change the data frequency on CSI interface,
because csi driver seems to be calculated the data frequency automatically.
but, the result was bad. No irq was happened in CSI_irqHandler after changed the config value(2->4).
I have a question. Is this possible to implement the CSI 4 data lanes at the S32V234 evb board with OV10640 sensor?
If it's possible,How can I implement the 4 data lane with OV10640 sensor?
the other question is that :
At S32 design studio s/w code, In case of MAXIM OV10640,application code seems to support this 4 data lanes case
typedef enum CSI_CameraType_t
{
CSI_NONE,
CSI_SONY224,
CSI_OV10640,
CSI_MAX_SONY224,
CSI_MAX_OV10640,
CSI_MAX_OV10635,
CSI_PAN34420
} CSI_CameraType_t;
What does MAX OV10640 mean? Can I use this procedure?