AnsweredAssumed Answered

PF3000 input power

Question asked by Noam Weidenfeld on May 28, 2017

Hi,

 

I am using the SMARC standard for SOM applications. The input power requirements are 3.0V to 5.25V.

Can I use the PF3000 for such input requirements? (I failed to understand the sentence " Input voltage range: 2.8 V to 4.5 V or 3.7 V to 5.5 V")

Thanks

Noam

Outcomes