AnsweredAssumed Answered

FXTH87 Datasheet Typo

Question asked by Lucas Cooter on May 23, 2017
Latest reply on May 30, 2017 by Lucas Cooter

Page 38, Table 25.

External Reset Pin

This bit indicates reset was caused by an active-low level on the external reset pin if the device was in either the STOP1 or RUN modes. This bit is not set if the external reset pin is pulled low when the device is in the STOP1 mode.
0 Reset not caused by external reset pin
1 Reset came from external reset pin

 

 

 

Sentence One Says: Bit is set in Stop1 Mode.

Sentence Two Says: Bit is NOT set in Stop1 Mode.

 

Sentence two contradicts sentence one. 

Which is it? Both of these sentences cannot be true.

Attachments

Outcomes