Not neccessary to swap u-boot and RCW for LS1012ARDB in SDK v2.0-1703

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not neccessary to swap u-boot and RCW for LS1012ARDB in SDK v2.0-1703

925 Views
chuckcorley
NXP Employee
NXP Employee

In the QorIQ SDK v2.0-1703 Documentation under "Deploy U-Boot, Linux Kernel, and Root Filesystem to a Reference Design Board (RDB)" for LS1012ARDB under Programming a New U-Boot, RCW, and PPA Firmware, it says "Note: RCW and U-Boot binary must be byte swapped using command (tclsh ./byte_swap.tcl u-boot-dtb.bin u-boot-dtb_swap.bin 8)".   This does not work and prevents the RDB from resetting.  Rumor says that was applicable to SDK v2.0-1701 but swapping is now done automatically in SDK v2.0-1703.  I did not independently confirm that.  But I do know that the default RCW and u-boot I built for SDK v2.0-1703 work successfully without swapping.

Labels (1)
Tags (1)
0 Kudos
1 Reply

617 Views
Pavel
NXP Employee
NXP Employee

You are right.

It is not needed.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos