why imx6solo can not boot from spi nor flash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why imx6solo can not boot from spi nor flash?

552 Views
翔李
Contributor IV

HI,

When my imx6solo board boot from spi nor flash32MB by standard operation,it is ok,but can not boot from dual spi,why?

Where is the code or driver to boot from dual spi nor falsh?

Thanks,boss  :smileyhappy:

pastedImage_1.png

0 Kudos
2 Replies

410 Views
igorpadykov
NXP Employee
NXP Employee

Hi

i.MX6S does not support boot from dual/quad spi, only single spi nor is supported.

Please refer to i.MX6SDL Reference Manual Table 8-23. SPI IOMUX Pin Configuration

for connections for spi-nor.

http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

410 Views
翔李
Contributor IV

Thanks。

But ago,someone said solo do not support quad-spi,but support dual spi.

Where is the reference design of imx6 solo? 

Also,I find that solo's RM pdf only has SPI IOMUX PIN configuration table,it is not show solo do not support dual or quad spi.but imx6-quad has quadspi chapter and do not show it support dual spi. I am missing.

pastedImage_3.png

pastedImage_4.png

pastedImage_2.png

0 Kudos