Dear All
Recently,I download the 'KEA128_BLDC_Sensorless' project from NXP ,and installed the BLDC function library'KEAx_AMMCLIB_v1.0.0' ,but the project is operated in codewarrior, I try to transplant the project to MDK and met some problems:
I find these FUNC without definition,so ,Can these functions be found in NXP website or other place?
In BLDC function library ,these FUNC only make a statement,but in codewarrior the project was right,I was a little confused..
so ,what problems do I need to be aware of in the transplant process? And the KEA128BLDC MDK project exist?where can I find it? or find functions that are undefined .
Thank u;
Eric