What is the max. spi clk of imx6 solo for spi nor flash boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the max. spi clk of imx6 solo for spi nor flash boot?

Jump to solution
834 Views
翔李
Contributor IV

HI

  On imx6 solo,My board boot from spi nor flash 32MB in standard or dual operation and solo not support quad spi.

  what the max. clk freq. of solo to boot from spi nor flash? Is it 60MHZ?And the flash is 104MHZ or 208MHZ for standard or dual spi.So,solo's spi clk is lower to spi nor flash?Pity.

  My flash isW25Q256FVEIG,winbond 32MBYTE SPI NOR FLASH.

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

0 Kudos
1 Solution
519 Views
Yuri
NXP Employee
NXP Employee

Hello,

  please look at the following Q&A: What is i.Mx6 ECSPI max frequency? 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

View solution in original post

2 Replies
520 Views
Yuri
NXP Employee
NXP Employee

Hello,

  please look at the following Q&A: What is i.Mx6 ECSPI max frequency? 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

519 Views
翔李
Contributor IV

From your link,It is only 60mhz for spi nor flash clk.

Thanks.

0 Kudos