Is there a way to use the S32K144x RTM SDK without Processor Expert?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a way to use the S32K144x RTM SDK without Processor Expert?

1,253 Views
andrewstroz
Contributor I

I have tried to link the SDK .c files and include the .h files with no luck. What would be the best way to use the SDK without processor expert? or is there no way to do this?

Labels (1)
0 Kudos
2 Replies

1,030 Views
jiri_kral
NXP Employee
NXP Employee

Hello Andrew, 

well - theoretically it is possible use RTM SDK without processor expert, but you have to manually write all the config structures used in SDK as argument in functions.

For what reason you want bypass processor expert?  

Jiri

0 Kudos

1,030 Views
andrewstroz
Contributor I

No specific reason, was just looking into the possibility.

0 Kudos