AnsweredAssumed Answered

PEMicro Selection is Greyed Out

Question asked by Jay Moskowitz on May 22, 2017
Latest reply on May 22, 2017 by ZhangJennie

I am using the Eclipse version of CW (10.1) for the HSC08 processor for the first time. I had been using the V5 Classic Version forever, but it no longer supports the processor. I used the Code Warrior Classic Project Importer to transfer my xxx.mcp project into CW 10.1.

 

The issue is that the along the command bar at the top, next to File, Edit, Refractors, etc. the entry called PEMicro is greyed out. We do use the PE Micro USB Multilink Universal to flash the HSC08 processor. So I am concerned that this is greyed out and I can't see any of the options for that selection.

 

Why might this entry be greyed out?

Outcomes