Bramini

Will newer LPCs appear with A5/A7 Cores?

Discussion created by Bramini on May 21, 2017
Latest reply on May 24, 2017 by soledad

I'm wondering if there will be in the future a product in the LPC line with a more advanced CPU, that it could be used for implementing a complete system. At the time of writing, it seems to me that only LPC3000 family provides something like that but, although an ARM9 with its MMU can do this task and run a true, protected OS, they are not at the same level of newer ICs like M4 with an FPU. Using a CPU like an A5/A7 with their more advanced capabilities (speed, VFPv4

and SIMD), near the well tested LPC peripherals into a friendly LQFP package would be great.

The additional option to have in some models a good amount of internal RAM (SDR? DDR?) for removing the extra space required for external memory chips would be also appreciated.

 

Thank you very much for your time.

 

Sincerely.

Outcomes