GStreamer-1.0 and imx6sx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GStreamer-1.0 and imx6sx

624 Views
adelantesey
Contributor IV

Dear All,

I have mx6sxsabresd with yocto linux 4.1.15, it has wayland compositor and i use weston as platform 

to run and debug qt applications through ssh.

qt forms applications work, but when I use gstreamer in qt (e.g. playbin) it plays only the audio! with out the graphics.

gst-inspect shows that i do not have waylandsink, in fact, $gst-inspect | grep wayland shows nothing! 

what do i need to play audio/video files on wayland/weston. or should i change the compositor?

Thank you in advanced 

Labels (2)
0 Kudos
1 Reply

437 Views
igorpadykov
NXP Employee
NXP Employee

Hi Adelante

i.MX6SX has not vpu and according to attached Release Notes sect.6.4 i.MX Qt Applications :

..applications are only available in platforms with VPU.."

Also please check Table 29. Video codec specification for hardware without VPU acceleration.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos