Dear All,
I have mx6sxsabresd with yocto linux 4.1.15, it has wayland compositor and i use weston as platform
to run and debug qt applications through ssh.
qt forms applications work, but when I use gstreamer in qt (e.g. playbin) it plays only the audio! with out the graphics.
gst-inspect shows that i do not have waylandsink, in fact, $gst-inspect | grep wayland shows nothing!
what do i need to play audio/video files on wayland/weston. or should i change the compositor?
Thank you in advanced
Hi Adelante
i.MX6SX has not vpu and according to attached Release Notes sect.6.4 i.MX Qt Applications :
..applications are only available in platforms with VPU.."
Also please check Table 29. Video codec specification for hardware without VPU acceleration.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------