MFRC522 and MFRC630

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFRC522 and MFRC630

3,588 Views
berniecheah
Contributor I

Hi,

May I know if mfrc630 is a drop in placement for 522? If not, which is the closest rfid reader that can replace mfrc522?

Tags (2)
0 Kudos
1 Reply

2,164 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Bernie,

    you can get the following information from our official website:

-----------------------------------------------------

MFRC522 is a highly integrated reader/writer IC for contactless communication at 13.56 MHz. The MFRC522 reader supports ISO/IEC 14443 A/MIFARE® and NTAG®. This part is not recommended for new design ins. For new designs we recommend MFRC630.

-----------------------------------------------------

So please select MFRC630 for new design!

MFRC522's package is the same as that of MFRC523, MFRC522 can be replaced with MFRC523.


Have a great day,
TIC   weidong sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos