Difference between QT on Linux and on Integrity RTOS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between QT on Linux and on Integrity RTOS?

Jump to solution
837 Views
maheshkumarkoda
Contributor III

Hallo,

I would like to know the difference between porting QT on Embedded Linux and on Integrity RTOS with Sabreauto board:

1). What are the compatible modules interfaced between Linux and QT framework?

for example : Wayland and X11?

2). How Integrity can be ported with QT?

Can Wayland , X11 be ported with integrity?

3). Is there any architectural diagram which explains Linux+QT port?

please provide if any.

Thanks,

Mahesh.

Labels (2)
0 Kudos
1 Solution
553 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

these are specific OS questions and may be posted on appropriate specialized forums like

http://qt-project.org/wiki/i.MX-6

Embedded Devices with Qt and the INTEGRITY RTOS - Qt Blog 

from hardware point of view, drivers are the same for these opearting systems

Best regards
igor
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
554 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

these are specific OS questions and may be posted on appropriate specialized forums like

http://qt-project.org/wiki/i.MX-6

Embedded Devices with Qt and the INTEGRITY RTOS - Qt Blog 

from hardware point of view, drivers are the same for these opearting systems

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos