Set Radio Power (JN5168-001-M06)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Set Radio Power (JN5168-001-M06)

590 Views
tssdev
Contributor I

Hello! 

I am using the AHI to interface with the radio, but I do not see a way to set the power level. I need to set the output power to the maximum that the radio can transmit.

First I run vAHI_HighPowerModuleEnable(1, 1) to set the radio in high power mode.

However, I do not then have a way to set the power. I found the call "bAHI_PhyRadioSetPower", but this fails in the linking step (even though other AHI functions work fine).

Unfortunately I know that I need to set a higher output because the signal only reaches a few dozen meters through open unobstructed space with my current settings.

Any help here would be appreciated. Thanks in advance!

Tags (1)
0 Kudos
2 Replies

382 Views
tssdev
Contributor I

Hello, just following up on this, waiting for a reply from NXP/Jennic.

Thanks!

0 Kudos

382 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

You enter this questions internally, and you got a reply.

Did you solve your issue?

Best Regards,

Mario

0 Kudos