Hi,
I'm using the P2020RDB-PCA board.
There are two I2C EEPROMs on this board, Boot EEPROM(U31) and BRD EEPROM(U51).
The question is, how can I get the hex file of the BRD EEPROM(U51)?
Best Regards,
Yang
The U51 binary image is attached.
To program the spd, load the spd image to memory, eg 0x1000000, run command:
eeprom write 52 1000000 0 80
which will program target I2C address 0x52, offset 0, length 0x80 from source 0x1000000.
Note: No need to erase the EEPROM before programming.
Thanks a lot !