SCM-i.MX 6SOLOX vs SoloX Sabre

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCM-i.MX 6SOLOX vs SoloX Sabre

433 Views
soumyaks
Contributor II

Hello,

I have to start building a product on imx6 SoloX processor. There are two options that comes.

1.  imx6 SX SabreSD evaluation kit

2.  SCM-i.MX 6SOLOX evaluation kit

Although the packaging is different, there are many similarities in the boards. Could someone point to what would be the software overhead for SabreSD vs SCM board?

Many Thanks,

Soumya

Labels (1)
0 Kudos
1 Reply

325 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems the bsp version for scm is L3.14.52, the latest version for 6sxevk board is L4.1.15_2.0.0

you can find the scm yocto bsp and nxp yocto bsp from the link I post

GitHub - juan-gutierrez/meta-nxp-imx-scm: SCM Yocto Meta layer

0 Kudos