AnsweredAssumed Answered

porting WEC7_v3.1.1.16(windows embedded compact) to iMX6Q SDB with sdcard

Question asked by bharath t s on May 10, 2017
Latest reply on May 15, 2017 by bharath t s

Hi ,

 

   i was porting WEC7 _v3.1.1.16 to imx6q SDB & have downloaded the images from https://witekio.com/cpu/i-mx-6/ (Adeneo Embedded) & i was loading binaries using CFimager from freescale to SD card & i was not able to see any logs on the serial monitor...

i have executed the following commands in windows10

    1. cfimager.exe -f NK.nb0 -d E -imx53 -a 
Inline image

   2.  cfimager.exe -f EBOOT.nb0 -d E -imx53

 

After this i switched on the board by setting Boot mode switch to sd card boot & i was not able to any logs.....

 

 

kindly help by giving full procedure to boot iMX6Q_SDB with WEC7 / WCE2013...

Outcomes