AnsweredAssumed Answered

porting WEC7_v3.1.1.16(windows embedded compact) to iMX6Q SDB

Question asked by bharath t s on May 10, 2017
Latest reply on May 11, 2017 by Bio_TICFSL

Hi ,

 

   i was porting WEC7 _v3.1.1.16 to imx6q SDB & have downloaded the images from https://witekio.com/cpu/i-mx-6/ (Adeneo Embedded) & i was loading binaries using MFGTool from freescale through USB boot & i was getting the below response with my formatedSD card(FAT) inserted to the board...


Inline image

 

as per the manual i was suppose to get these logs...

Inline image

 

 Once loading these binaries i changed the Boot mode switch to SD card Boot & i was NOT ABLE TO SEE ANY LOGS ON Serial monitor...

 

kindly help by giving full procedure to boot iMX6Q_SDB with WEC7...

Outcomes