Debug error in s32 project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug error in s32 project

1,655 Views
vrushalitaklika
Contributor III

I am debugging a s32 project for MPC5777C MCU.

Attached is the error. Please suggest solution

Labels (1)
0 Kudos
2 Replies

1,032 Views
stanish
NXP Employee
NXP Employee

Hi,

It looks like some there is an issue with the debug configuration.

Can you check the executable line in GDB Client settings panel:

pastedImage_2.png

As a general suggestion I'd recommend you to try to create a new project for MPC5777C build it and debug.

Does this empty project works on your side?

Stan

0 Kudos

1,032 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please clarify me following points?

1) Have you already installed update1?

S32 Design Studio for Power v1.1 - Update 1 available 

2) Which debug probe you use?

3) Have you ever been able to connect to this microcontroller or to different one?

Make sure you do not have opened any other S32DS instance which also uses GDB server or any other application which uses GDB server.

Then please look at the thread below and update PeMicro debug interface (if you have already don't do that)

https://community.nxp.com/thread/448305 

You can also try to uninstall Design Studio and install it one again together with update1 and PeMicro update.

Please let me know if my suggestions help you.

Regards,

Martin

0 Kudos