AnsweredAssumed Answered

LPC4370 and  S25FL256SAGMFI0001 Flash Algorithm

Question asked by sujay p on May 9, 2017
Latest reply on May 11, 2017 by soledad

Dear NXP Technical Support Services ,

 

I am writing in regards the programming of the  the keil ulink pro and i was getting some errors which is as follows:-

 

 *** Using Compiler 'V5.06 update 1 (build 61)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'
Build target 'Target 1'
".\Objects\Example_42_88.axf" - 0 Error(s), 0 Warning(s).
Build Time Elapsed:  00:00:00
Load "E:\\Microvision_projects\\Objects\\Example_42_88.axf"
No Algorithm found for: 00000000H - 0000114BH
Erase skipped!
Error: Flash Download failed  -  "Cortex-M4"
Flash Load finished at 18:29:19

 

I think the cortex M4 Device selection requires some configuration for  the  SPIFI  Flash programming algorithm and requires  the configuration using the Settings.

 

May be I require S25FL256SAGMFI0001 Flash Algorithm drivers which is not found in the Keil MDK.

 

I am using LPC4370FET256 microcontroller interfaced with the external flash memory SPIFI flash memory S25FL256SAGMFI0001 and will you  please help in this regards.

 

Regards
Sujay

Outcomes