AnsweredAssumed Answered

Download the images into the MMC on Ubuntu12.04

Question asked by Jerry Lee on May 4, 2017
Latest reply on May 11, 2017 by florian koenig

when I Download the images(IMX6Q) into the MMC on Ubuntu12.04,

I used cmd :$ sudo dd if=u-boot.imx of= /dev/sdx bs=1K seek=1; sync
but I can not find /dev/sdx.

I have found mmc\SD card can not be loaded under Ubuntu12.04 system,
But I can use the MFGTOOS in Windows to download the firmware to the board
May I ask what is the reason
How can i solve it?

Outcomes