AnsweredAssumed Answered

FRDM-KW41Z (Flash resident bootloader): Thread Reset (in 3 min)

Question asked by sensenthuran on May 4, 2017
Latest reply on Jun 5, 2017 by Rote Chen

I am having one issue with “Thread version 1.1.1.15 - thread_host_controlled_device_freertos”. When I loaded to FRDM KW41Z (has Flash resident bootloader), It resets after 3mins. 

 

I did the memory map as below

C:\MCUXpressoIDE_10.0.0_344\workspace\frdmkw41z_wireless_examples_thread_host_controlled_device_freertos\source\MKW41Z512xxx4_connectivity.ld

__region_ROM_start__   =  (0x00004000); //  default: 0x00000000

m_flash_config_start = (0x4400); //  default: 0x400

m_flash_config_end   = (0x4410); //  default: 0x410

 

Do you think, the “flash resident” bootloader is still valid for Thread version 1.1.1.15 ?

 

With the SDK_2.2_FRDM-KW41Z, I can see only
1) OTAP Bootloader and
2) FSCI Bootloader
But not “flash resident” bootloader Juan Carlos Pacheco

 

Thanks 

Outcomes