Hi ,
We are using the Nxp P2020RDB Board , the thing is we able to write and read Nand flash ,but Booting is not happen what could be the problem ,NOR Flash boot is working fine, what could be the problem ? Please suggest me
NAND Flash part no (MT29F1G08ABAEAWP-IT:E)
SDK version 1.7
After loading the loading images into the Nand flash , it will show in the console
"secondary programming load error......read failed"
Regards
Naresh
have a nice day.
Hello naresh puli,
Please try the following procedure.
Please set up u-boot from NOR flash, then program the attached image to NAND flash with the following commands.
=>tftp 1000000 u-boot-nand-P2020RDB-PC_NAND.bin
=>nand erase 0 +$filesize
=>nand write 1000000 0 $filesize
Then power off the target board, configure the switch settings as the following and power on the board again.
SW3[1~6] = 111010
If your problem remains, please feel free to let me know.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yiping Wang,
i hope you are doing good...
i am not able to find where is the attached image, pls attach the only binary file.Hi Andrei.skok,
Thanks for you supporting .but After loading the loading image into the Nand flash , it will show in the console
"secondary programming load error......read failed"
Regards
Naresh
Hello Naresh,
Please provide the whole u-boot console log.
Thanks,
Yiping
Hi,
Write and read is happening , but when i load U-boot image it doesn't boot from NAND Boot
nand info
Device 0: nand0, sector size 128 KiB
Page size 2048 b
OOB size 64 b
Erase size 131072 b
tftp 1000000 test-file
Using eTSEC1 device
TFTP from server 9.1.1.7; our IP address is 9.1.1.45
Filename 'test-file'.
Load address: 0x1000000
Loading: #
1000 Bytes/s
done
Bytes transferred = 52 (34 hex)
=> nand write 1000000 0 34
NAND write: device 0 offset 0x0, size 0x34
52 bytes written: OK
cmp 1000000 2000000 34
word at 0x01000034 (0x4d122082) != word at 0x02000034 (0x+-----------------------------+
Total of 13 word(s) were the same | |
=> md 2000000 10
02000000: 4e616e64 20546573 74696e67 0a48656c Argus Testing.He
02000010: 6c6f2077 6f726c64 0a313233 34353637 llo world.123456
02000020: 38393061 62636465 66676869 6a6b6c6d 7890abcdefghijkl
02000030: 6e6f700a 5ce1abb2 d4f9e57c 9fe9ff0f mnop.\......|...
=> md 1000000 10
01000000: 4e616e64 20546573 74696e67 0a48656c Argus Testing.He
01000010: 6c6f2077 6f726c64 0a313233 34353637 llo world.123456
01000020: 38393061 62636465 66676869 6a6b6c6d 7890abcdefghijkl
01000030: 6e6f700a 4d122082 1861c1c0 0282001c mnop.M. ..a.....
After loading the loading images into the Nand flash , i change the switch settings to 11101010
i am getting only this single statement , in the log file. what could be the problem?
"secondary programming load error......read failed"
Hi Yiping Wang,
where did you attached the image , i didn't find pls attach the only binary file.
Hi Yiping Wang,
i hope you are doing good...
Still the Nand Boot problem is there.
Spi chip is not detecting(Part no S25FL128P0XNFI00) , when i give the command is showing like un supported flsah IDs
sf probe
SF: Unsupported flash IDs: manuf ff, jedec ffff, ext_jedec ffff
Failed to initialize SPI flash at 0:0
what could be the problem , how can i come out problems pls suggest me.
Regards
Naresh
Have a great day .