Does anybody know the accuracy and range of the temp diode for P2020 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does anybody know the accuracy and range of the temp diode for P2020 ?

480 Views
davidflores
Contributor I

Read the spec sheet and is know where in it.

0 Kudos
2 Replies

352 Views
andrei_skok
NXP Employee
NXP Employee

Some helpful information can be found in the AN4787

https://www.nxp.com/webapp/Download?colCode=AN4787 

0 Kudos

352 Views
andrei_skok
NXP Employee
NXP Employee

All available information for the temp diode can be found in the P2020 Datasheet:

3.2 Temperature Diode
The device has a temperature diode on the microprocessor that can be used in conjunction with other system temperature
monitoring devices. These devices use the negative temperature coefficient of a diode operated at a constant current to
determine the temperature of the microprocessor and its environment.
The following are the specifications of the P2020 on-board temperature diode:
Operating range: 10 – 230 μA
Ideality factor over 13.5 – 220 μA; n = 1.011 +/- 0.008

It is valid within operating temperature range -40C - +125C

0 Kudos