寻找PN7462Android驱动资料

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

寻找PN7462Android驱动资料

1,378 Views
13102370205
Contributor I

有没有PN7462的Android驱动资料?

0 Kudos
2 Replies

1,188 Views
weidong_sun
NXP TechSupport
NXP TechSupport

你好,小雨,

    我们没有发行PN7462的android驱动程序,如果你需要在android下使用NFC,建议你使用PN7150,工程师可以使用android NFC SDK编写应用程序。libnfc-nci, HAL,及其驱动程序,android里面都已经支持,但是请注意一下android版本,在PN7150的文档里有说明。

    如果你一定要使用PN7462,你需要自己做移植,下面是个人的一些建议:

---如使用SPI接口和处理器连接

请用spidev.c驱动PN7462,在spidev.c里提供上层接口就可以对寄存器读写了,这样做起来比较简单。

Best Regards,

Weidong

0 Kudos

1,188 Views
13102370205
Contributor I

你好,weidong

我们选择PN7462主要是因为PN7462能够管理nfc和SAM卡,如果我们使用PN7150,就只具备nfc的功能。您能不能为我们提供一个方案在使用PN7150的同时,还能够管理SAM卡.

13102370205@163.com

发件人: weidong.sun

发送时间: 2017-05-03 14:35

收件人: 小雨 李

主题: Re: - Re: 寻找PN7462Android驱动资料

NXP Community

Re: 寻找PN7462Android驱动资料

reply from Wigros Sun in NFC - View the full discussion

你好,小雨,

我们没有发行PN7462的android驱动程序,如果你需要在android下使用NFC,建议你使用PN7150,工程师可以使用android NFC SDK编写应用程序。libnfc-nci, HAL,及其驱动程序,android里面都已经支持,但是请注意一下android版本,在PN7150的文档里有说明。

如果你一定要使用PN7462,你需要自己做移植,下面是个人的一些建议:

---如使用SPI接口和处理器连接

请用spidev.c驱动PN7462,在spidev.c里提供上层接口就可以对寄存器读写了,这样做起来比较简单。

Best Regards,

Weidong

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in NFC by email or at NXP Community

Following Re: 寻找PN7462Android驱动资料 in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos