SLRC61002HN register access?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SLRC61002HN register access?

743 Views
Breeze
Contributor II

Hi Expert,

We use KL17 SPI interface with SLRC61002HN for the register check. Found that the SPI read is functional, For example,

Read 46h --> Response with 6eh , it matches the external IFSEL1="hi", IFSEL0="lo"

But no matter what command we write, the register seems not functional. For example, 

Read 03h --> Response with 05h, then Write 03h 1fh --> Read 03h again, the result is still 05h, not 1fh we expect.

Is any command step we have to follow?

 Thanks,

Gilbert

0 Kudos
1 Reply

653 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Gilbert,

Would you please refer to 7.4.2 SPI interface of the data sheet http://www.nxp.com/documents/data_sheet/SLRC610.pdf  and check if you have implemented the SPI transfer correctly? For example, the NSS control, the address byte setting, read/write timing and byte order, etc.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos